motors
Ironhorse™ DC Motors
shop now
flange kit
DC Gearmotor brushes
Brushes commutate the incoming current in a DC motor. All IronHorse PMDC motors are shipped with a set of brushes in the motor. An extra set of brushes is included in the box. The brushes below can be ordered as spares.
IronHorse DC brushes should be changed at a maximum interval of 2500 hours motor runtime. When changing brushes, always change them as a set (never change only one brush).
These replacement parts also fit many AutomationDirect small-frame DC motors. Refer to the DC Motors section for small-frame motor application information.
DC Gearmotor Accessories
Part Number For Gearmotors Price Description